Post Go back to editing

ADSP-2148x E-pad question

Hello

I have just finished reading the EE- 352 Engineering note regarding E-pad packages and mounting techniques. One thing I am not clear of is you don't say whether or not you use thermal relief's or direct connects on the ground plane connecting via's. Obviously direct connection would give you better electrical connection and lower thermal resistance to the ground plane but would it alter the temperature profile needed for reflow ? ie which would be better from the point of view of manufacturability ?

regards

david

Parents
  • Hello Al

    Regarding the 2mm hole how do you solder it ? Do you plug up the hole with solder paster and hit it with a hot air gun until it reflows or do you use a narrow tip, heat up the hole a bit and then feed in solder into the hole ? If you use a soldering iron what size tip and temperature do you use ?

    regards

    david

Reply
  • Hello Al

    Regarding the 2mm hole how do you solder it ? Do you plug up the hole with solder paster and hit it with a hot air gun until it reflows or do you use a narrow tip, heat up the hole a bit and then feed in solder into the hole ? If you use a soldering iron what size tip and temperature do you use ?

    regards

    david

Children
No Data