Hi everybody!
Please help in my case
Ive triying to establish valid data reading from LTC4151
At first I decided to R/W in TEST MODE
So I do the following!
- 1 Set 7 bit address, 80 kHz bit rate
- Store to control register 0x10 to set up TEST UP
- Store to MSB of SENSE register 0x55
- Store to LSB of SENSE resgister 0xAA
- Read MSB of SENSE register - and IC get 0x55
- Read LSB of SENSE reister - and IC get 0x55 instead of 0xAA
The same situation at the reast pair of register (in TEST MODE)
And then I read control register before READ MSB and LSB of SENSE register it also gets 0x55 instead of 0x10
Please help, I didin understand
I chek all by oscilosope and what it gets:
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACKb7b6b5b4b3b2b1b0ACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 1 1 0 0 0 0 0 1 0 0 0 0 0
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACKb7b6b5b4b3b2b1b0ACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 0 0 0 0 0 1 0 1 0 1 0 1 0
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACKb7b6b5b4b3b2b1b0ACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 1 1 0 0 0 0 0 1 0 0 0 0 0
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACKb7b6b5b4b3b2b1b0ACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 0 0 1 0 1 0 1 0 1 0 1 0 0
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACK//S//a6a5a4a3a2a1a0r/nWACKb7b6b5b4b3b2b1b0nACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 0 0 0 0 1 1 0 0 1 1 1 1 0 0 1 0 1 0 1 0 1 1
a6a5a4a3a2a1a0R/nWACKb7b6b5b4b3b2b1b0ACK//S//a6a5a4a3a2a1a0r/nWACKb7b6b5b4b3b2b1b0nACK
1 1 0 0 1 1 1 0 0 0 0 0 0 0 0 0 1 0 1 1 0 0 1 1 1 1 0 0 1 0 1 0 1 0 1 1