ADP5070 sepic circuit sees overcurrent condition

Hi guys,
I'M using a ADP5070 from analog device to generate a +8V and a -4V . The circuit for the -4V works fine. As for the +8V it does not.
The circuit used is a SEPIC topology. You can see the circuit schematic in the pictures linked(sepic.png).
The behavior I am observing is that the ADP5070's over current condition keeps getting trigged . I used an oscilloscope to probe at the indutctance's pins and what I see is that the circuit switches for a certain period of time and after that nothing happens for about 32ms (picture linked sw1.png). When reading about this in the datasheets it says that this timeout is due to an overcurrent condition in the switch node. (current_sense.pgn,current_sense2.pgn,reset_time.png)
Does anyone have an idea why I might have an over current condition? I've simulated my circuit before designing it and in simulation it worked just fine.
I've also tried to use the soft start of the circuit by adding a 100k resistor. Strangely my restart delay increased by 150ms while I was expecting a 20 ms increase(reset_time.png), and unfortunately it did not solve my problem (softstrt.pgn)..
Thanks for the help guys

Sepic.png

current_sense.png

current_sense2.pgn

reset_time.png

softstrt.pgn

sw1.png

Top Replies

Parents Reply
  • 0
    •  Analog Employees 
    on Jul 23, 2021 8:00 AM in reply to ovi08

    Sorry for long delay. It would be faster if you send me email. I can't exactly tell what's going on until you send me more waveforms including zoomed in version of several nodes. I would recommend that you use our ADIsimPower tool to generate the right component values. Make sure you have the right compensation components too to ensure good start-up performance.

Children
No Data