Post Go back to editing

Lt3763 drive a 10A LD

I want to use lt3763 drive a LD,24v input,4v output,current is 10A,how to choose a right Rc,Cc,Fsw,datasheet just have 12v input,I am confuse about also those Rc,Cc,Fsw is suitable for 24v input,thanks ,

Parents Reply
  • Refer to FET safe operating area. If the overshoot exceed FET rating, then it is not good. VSW spikes on scope shots can be artifacts based on your testing setup. Also, key is PCB layout of your switching converter. Main loops should be tights. We have layout guideline in datasheet and technical article you can find. Please refer to demo board as good reference design.

Children
  • hi,i have a question about i want to drive a low power LD,maybe just have 100mA or 200mA,Can this chip accurately drive the laser? because in my mind ,LT3763 Suitable for driving high-power LED or LD,If not suitable for drive a low power LD,Can you recommend a suitable LED driver chip for me?how about LT3474?thank you very much Slight smile

  • hi,i have a question about i want to drive a low power LD,maybe just have 100mA or 200mA,Can this chip accurately drive the laser? because in my mind ,LT3763 Suitable for driving high-power LED or LD,If not suitable for drive a low power LD,Can you recommend a suitable LED driver chip for me?how about LT3474?thank you very much Slight smile