Post Go back to editing

ADM106x Headerfile

Hello

I´ve to program a ADM1062 for a project.

And now my idea was to write a headerfile thats offer me the possibility to write something like

VP1.PS1OVTH = 0;

VP1.SFDV1CFG = 10US;

Has someone allready made a headerfile with this definesor something similar. I don´t want to write 100 or more macros.

Thanks in advance

René

Parents
  • Hi Ren

    On a longer powersupply line I have 5, 6 or maybe more devices with a ADM1062 and the ADM should control the voltage over the bus.

    For this I need to configure the ADM1062 over a microcontroller. At powerup the system looks at the powerlevel, measure it and that are the reference value. If the power go down (maybe 10%) there should raise a pin at the ADM1062 for the microcontroller.

    I ´ve not only one voltage, I´ve 7.

    Thats the reason that I need to configure the ADM online.

    René

Reply
  • Hi Ren

    On a longer powersupply line I have 5, 6 or maybe more devices with a ADM1062 and the ADM should control the voltage over the bus.

    For this I need to configure the ADM1062 over a microcontroller. At powerup the system looks at the powerlevel, measure it and that are the reference value. If the power go down (maybe 10%) there should raise a pin at the ADM1062 for the microcontroller.

    I ´ve not only one voltage, I´ve 7.

    Thats the reason that I need to configure the ADM online.

    René

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.