HI All:
I want to use LT3383 to get a output about 5A, can LT3383 achieve it? If ok(combine the two 2.5A output), any reference design?
LT3383
Recommended for New Designs
The LT3383 is a complete power management solution for advanced portable application processor-based systems. The device contains four synchronous step...
Datasheet
LT3383 on Analog.com
HI All:
I want to use LT3383 to get a output about 5A, can LT3383 achieve it? If ok(combine the two 2.5A output), any reference design?
Hi,
Unfortunately LT3383 does not support paralleling multiple channels. It does not have the multiphase feature, and the two channels are not out of phase.
It might be possible to parallel general power supply in this method shown below:

However, the accuracy of the output might suffer. The balance resistor will also introduce extra loss. The balance of the two channels also depends on the value of the two balance resistors. I do not recommend this method when your total output current is twice as the max current output of a single channel.
Thanks,
Wenwei.
Hi,
Unfortunately LT3383 does not support paralleling multiple channels. It does not have the multiphase feature, and the two channels are not out of phase.
It might be possible to parallel general power supply in this method shown below:

However, the accuracy of the output might suffer. The balance resistor will also introduce extra loss. The balance of the two channels also depends on the value of the two balance resistors. I do not recommend this method when your total output current is twice as the max current output of a single channel.
Thanks,
Wenwei.