Post Go back to editing

ADP2120 operating in a discontinuous mode when synchronized.

I have an ADP2120 circuit that is operating it what looks like a discontinuous mode, but is synchronized to an input clock.

The circuit is a 5V to 3.3 V circuit using the component values I got from ADIsimPower. The current draw on the 3.3V varies vs time. The switch waveform has an odd ring that moves around. The switch turns on (0V out) for ~200 ns, then softly releases and slews up to ~4V, then drops to 3.5V before sharply turning off (5V). The switch waveform looks a little like the DCM (discontinuous conduction mode) in the data sheet, but with only a single broad ring. The circuit is synchronized to to a 1.2MHz clock (3.3V) so it shouldn't try to go to the PFM mode.

I haven't found any info about the DCM in the ADI web site yet. I have another ADP2120 operating at 5V to 1.4V that behaves nearly ideally. Any ideas or suggestions as to what this is & how to make it operate in the continuous conduction mode?

Parents
  • Kevin,

    thanks for the pictures, this is indeed DCM and if the part was synchronizing correctly then it would be operating in CCM.

    I would be interested to see if you force MODE pin high always if the part goes to CCM or not. Also when synchronized I would be interested in seeying what is the delay between the synch and the SW transition.

    I do not have an explanation for what you are seeying, how many boards have you built? do they all behave the same?

    Do you have R1 between PVIN and VIN? have you probed pin 1?

    LucaV

Reply
  • Kevin,

    thanks for the pictures, this is indeed DCM and if the part was synchronizing correctly then it would be operating in CCM.

    I would be interested to see if you force MODE pin high always if the part goes to CCM or not. Also when synchronized I would be interested in seeying what is the delay between the synch and the SW transition.

    I do not have an explanation for what you are seeying, how many boards have you built? do they all behave the same?

    Do you have R1 between PVIN and VIN? have you probed pin 1?

    LucaV

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.