Post Go back to editing

ADP2120 operating in a discontinuous mode when synchronized.

I have an ADP2120 circuit that is operating it what looks like a discontinuous mode, but is synchronized to an input clock.

The circuit is a 5V to 3.3 V circuit using the component values I got from ADIsimPower. The current draw on the 3.3V varies vs time. The switch waveform has an odd ring that moves around. The switch turns on (0V out) for ~200 ns, then softly releases and slews up to ~4V, then drops to 3.5V before sharply turning off (5V). The switch waveform looks a little like the DCM (discontinuous conduction mode) in the data sheet, but with only a single broad ring. The circuit is synchronized to to a 1.2MHz clock (3.3V) so it shouldn't try to go to the PFM mode.

I haven't found any info about the DCM in the ADI web site yet. I have another ADP2120 operating at 5V to 1.4V that behaves nearly ideally. Any ideas or suggestions as to what this is & how to make it operate in the continuous conduction mode?

Parents
  • The circuit is synchronizing correctly. The schematic is essentially the same as the application circuit in the data sheet (figure 50) with L= 2.2uH inductor, Cin = 2x 1u, Cout = 2x 10u. The circuit appears to be operating in the Discontinuous conduction mode, not the PFM mode. I've inserted a couple scope shots of the switch waveforms.

    As is, the circuit is generating a lot of low frequency noise. I believe this is due to the varying pulse width modulation. I want to get it to operate in the Continuous conduction mode where there should be less modulation of the inductor current. I *think* that increasing the inductor value should accomplish this. I would appreciate any info or links to any ADI documents that can offer insite into this.

Reply
  • The circuit is synchronizing correctly. The schematic is essentially the same as the application circuit in the data sheet (figure 50) with L= 2.2uH inductor, Cin = 2x 1u, Cout = 2x 10u. The circuit appears to be operating in the Discontinuous conduction mode, not the PFM mode. I've inserted a couple scope shots of the switch waveforms.

    As is, the circuit is generating a lot of low frequency noise. I believe this is due to the varying pulse width modulation. I want to get it to operate in the Continuous conduction mode where there should be less modulation of the inductor current. I *think* that increasing the inductor value should accomplish this. I would appreciate any info or links to any ADI documents that can offer insite into this.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.