Post Go back to editing

ADP2120 operating in a discontinuous mode when synchronized.

I have an ADP2120 circuit that is operating it what looks like a discontinuous mode, but is synchronized to an input clock.

The circuit is a 5V to 3.3 V circuit using the component values I got from ADIsimPower. The current draw on the 3.3V varies vs time. The switch waveform has an odd ring that moves around. The switch turns on (0V out) for ~200 ns, then softly releases and slews up to ~4V, then drops to 3.5V before sharply turning off (5V). The switch waveform looks a little like the DCM (discontinuous conduction mode) in the data sheet, but with only a single broad ring. The circuit is synchronized to to a 1.2MHz clock (3.3V) so it shouldn't try to go to the PFM mode.

I haven't found any info about the DCM in the ADI web site yet. I have another ADP2120 operating at 5V to 1.4V that behaves nearly ideally. Any ideas or suggestions as to what this is & how to make it operate in the continuous conduction mode?

Kevin,

A schematics, from your schematics,  some scope plots (VIN,  SW, Vout) would be great to have to be able to help you.

LucaV

  • If the ADP2120 is not synchronizing maybe your clock source is not compliant with the specs.

    100ns min pulse and VH=1.3V, VL=0.4V

    LucaV

  • The circuit is synchronizing correctly. The schematic is essentially the same as the application circuit in the data sheet (figure 50) with L= 2.2uH inductor, Cin = 2x 1u, Cout = 2x 10u. The circuit appears to be operating in the Discontinuous conduction mode, not the PFM mode. I've inserted a couple scope shots of the switch waveforms.

    As is, the circuit is generating a lot of low frequency noise. I believe this is due to the varying pulse width modulation. I want to get it to operate in the Continuous conduction mode where there should be less modulation of the inductor current. I *think* that increasing the inductor value should accomplish this. I would appreciate any info or links to any ADI documents that can offer insite into this.

  • Kevin,

    thanks for the pictures, this is indeed DCM and if the part was synchronizing correctly then it would be operating in CCM.

    I would be interested to see if you force MODE pin high always if the part goes to CCM or not. Also when synchronized I would be interested in seeying what is the delay between the synch and the SW transition.

    I do not have an explanation for what you are seeying, how many boards have you built? do they all behave the same?

    Do you have R1 between PVIN and VIN? have you probed pin 1?

    LucaV

  • I have the normal 10 ohm resistor between PVIN & VIN. Pin 1 looks pretty

    stable; some hash but no major ripple.

    What I believe is happening is that the stored energy in the inductors

    magnetic field has completely discharged into the output capacitors

    before the PWM cycle ends. At that point the the internal diode stops

    conducting and the switch voltage moves slowly to the output voltage.

    Increasing the output load makes the switching waveform look pretty much

    ideal (CCM). Doubling the inductance also does, I guess by making it

    take longer to energize/de-energize the inductors magnetic field.

    Is there a limit to the inductor size? The data sheet lists an extremely

    limited range (table 5 & 6) of 1 - 2.2 uH. Is there any problem using a

    4.7 - 6.8 uH inductor?

    Kevin McKee

    Project Manager

    Stanford Research Systems

    1290-D Reamwood Ave

    Sunnyvale, CA 94089

    408-744-9047, x237

  • Kevin,

    your description would be accurate if the part did not support CCM. I have the feeling your IC is not soldered well and the Sync pin is not getting the signal. How many boards have you built? As you described above the 1.4V part works as expected so there is something going on with this 3.3V design.

    The part has internal compensation and it designed to be stable with that range of inductors.

    LucaV

  • Luca,

    The part is perfectly synchronized, with the falling edge of the switch

    waveform perfectly stable. But there may be an issue with the part or

    soldering since 2 other boards do not exhibit this behavior.

    Of course the first board you check always behaves weirdly.

    Kevin McKee

    Project Manager

    Stanford Research Systems

    1290-D Reamwood Ave

    Sunnyvale, CA 94089

    408-744-9047, x237

  • Thanks for confirming my suspicion and good luck with the project.

    LucaV