Post Go back to editing

ADP2300 - can I use 'EN' PIN to connect to external PWM source (~20kHz)?

Hello,

I would like to use 'EN' pin to control externally the output by connect it to 50% PWN source (uP 3.3V).

And switch to PWM 100% only in specific cases.

The external PWM source will have constant frequency  ~20kHz.

May i connect it to 'EN" without any consequences?

The output voltage will be set to 2V and current shall be ~300mA.at that voltage

best regards

M.M.