Post Go back to editing

how do i decrease Iq with adp160

Hello Sir,

i have designed a power supply circuit based on ADP160AUJZ-3.0, the circuit diagram is below

PWR_BATT is Vin = 4.5V

PWR_RTC is Vout = 3.0V

The result is:

1. when load current is 3uA, Iq = 87uA

2. when no load on output port, Iq > 80uA

3. if  i  cut pin 3 from Vin, and connected  to gnd, Iq < 1uA

So i think there must be something wrong with my design. because Iq is more great than spec..

Please help me, thank you.

Parents Reply Children
No Data