Post Go back to editing

how do i decrease Iq with adp160

Hello Sir,

i have designed a power supply circuit based on ADP160AUJZ-3.0, the circuit diagram is below

PWR_BATT is Vin = 4.5V

PWR_RTC is Vout = 3.0V

The result is:

1. when load current is 3uA, Iq = 87uA

2. when no load on output port, Iq > 80uA

3. if  i  cut pin 3 from Vin, and connected  to gnd, Iq < 1uA

So i think there must be something wrong with my design. because Iq is more great than spec..

Please help me, thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.