Post Go back to editing

LTC4352 behavior when input power supply is low

Hello,

I have a question regarding how the LTC4352 Ideal Diode Controller will behave when the voltage at Vin is less than the 2.9V limit specified in the datasheet.  The circuit is not utilizing the under-voltage feature and the nominal rail voltage will be greater than the 2.9V limit.  There are two back to back FETs since the over-voltage feature is being utilized.  This scenario would only occur if the upstream power supply suffered some sort of fault.

I simulated the scenario using LTSpice and it appeared that the device remained in a Off/Low-power state with the FETs disabled.  Is this the correct/expected behavior for the described scenario?

Thank You.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.