Post Go back to editing

LTM4626 operating frequency setting

Thread Summary

The user asked how to calculate Rfset to modify the operating frequency of the LTM4626 and inquired about the function of a resistor between FREQ and INTVCC. The final answer clarified that the resistor Rfset is connected in parallel with 274kΩ to modify the frequency, and a direct connection between FREQ and INTVCC selects the maximum frequency of 3MHz. The accompanying answer noted that the LTM4626 datasheet (Rev B) does not include the frequency table, and the maximum frequency is 3MHz, not 800kHz.
AI Generated Content

Hello,

I don't unterstand the how to calculate Rfset to modify operating frequency.

The datasheet gives with Rset connected between FREQ and GND :

Does it mean 274KOhm in parallel with Rfset ?

An other point is : on eval board, FREQ pin can be connected  with a resistor to GND and another to INTVCC.

What is the function of the resistor between FREQ and INTVCC ?

Best regards

Parents Reply Children