How do I set up the Buck-Boost Output of the ADP5360?

How do I set up the Buck-Boost Output of the ADP5360?

Is there a table that shows the binary code that corresponds to the output voltage?

Thanks

Charly

Parents
  • +1
    •  Analog Employees 
    on May 3, 2021 2:25 PM

    Here is a table that showcases how it's done:

    BIN

    DEC

    Vout

    BIN

    DEC

    Vout

    0

    0

    1.8

    100000

    32

    3.95

    1

    1

    1.9

    100001

    33

    4

    10

    2

    2

    100010

    34

    4.05

    11

    3

    2.1

    100011

    35

    4.1

    100

    4

    2.2

    100100

    36

    4.15

    101

    5

    2.3

    100101

    37

    4.2

    110

    6

    2.4

    100110

    38

    4.25

    111

    7

    2.5

    100111

    39

    4.3

    1000

    8

    2.6

    101000

    40

    4.35

    1001

    9

    2.7

    101001

    41

    4.4

    1010

    10

    2.8

    101010

    42

    4.45

    1011

    11

    2.9

    101011

    43

    4.5

    1100

    12

    2.95

    101100

    44

    4.55

    1101

    13

    3

    101101

    45

    4.6

    1110

    14

    3.05

    101110

    46

    4.65

    1111

    15

    3.1

    101111

    47

    4.7

    10000

    16

    3.15

    110000

    48

    4.75

    10001

    17

    3.2

    110001

    49

    4.8

    10010

    18

    3.25

    110010

    50

    4.85

    10011

    19

    3.3

    110011

    51

    4.9

    10100

    20

    3.35

    110100

    52

    4.95

    10101

    21

    3.4

    110101

    53

    5

    10110

    22

    3.45

    110110

    54

    5.05

    10111

    23

    3.5

    110111

    55

    5.1

    11000

    24

    3.55

    111000

    56

    5.15

    11001

    25

    3.6

    111001

    57

    5.2

    11010

    26

    3.65

    111010

    58

    5.25

    11011

    27

    3.7

    111011

    59

    5.3

    11100

    28

    3.75

    111100

    60

    5.35

    11101

    29

    3.8

    111101

    61

    5.4

    11110

    30

    3.85

    111110

    62

    5.45

    11111

    31

    3.9

    111111

    63

    5.5

Reply
  • +1
    •  Analog Employees 
    on May 3, 2021 2:25 PM

    Here is a table that showcases how it's done:

    BIN

    DEC

    Vout

    BIN

    DEC

    Vout

    0

    0

    1.8

    100000

    32

    3.95

    1

    1

    1.9

    100001

    33

    4

    10

    2

    2

    100010

    34

    4.05

    11

    3

    2.1

    100011

    35

    4.1

    100

    4

    2.2

    100100

    36

    4.15

    101

    5

    2.3

    100101

    37

    4.2

    110

    6

    2.4

    100110

    38

    4.25

    111

    7

    2.5

    100111

    39

    4.3

    1000

    8

    2.6

    101000

    40

    4.35

    1001

    9

    2.7

    101001

    41

    4.4

    1010

    10

    2.8

    101010

    42

    4.45

    1011

    11

    2.9

    101011

    43

    4.5

    1100

    12

    2.95

    101100

    44

    4.55

    1101

    13

    3

    101101

    45

    4.6

    1110

    14

    3.05

    101110

    46

    4.65

    1111

    15

    3.1

    101111

    47

    4.7

    10000

    16

    3.15

    110000

    48

    4.75

    10001

    17

    3.2

    110001

    49

    4.8

    10010

    18

    3.25

    110010

    50

    4.85

    10011

    19

    3.3

    110011

    51

    4.9

    10100

    20

    3.35

    110100

    52

    4.95

    10101

    21

    3.4

    110101

    53

    5

    10110

    22

    3.45

    110110

    54

    5.05

    10111

    23

    3.5

    110111

    55

    5.1

    11000

    24

    3.55

    111000

    56

    5.15

    11001

    25

    3.6

    111001

    57

    5.2

    11010

    26

    3.65

    111010

    58

    5.25

    11011

    27

    3.7

    111011

    59

    5.3

    11100

    28

    3.75

    111100

    60

    5.35

    11101

    29

    3.8

    111101

    61

    5.4

    11110

    30

    3.85

    111110

    62

    5.45

    11111

    31

    3.9

    111111

    63

    5.5

Children
No Data