Post Go back to editing

LT1764A vs. LT1764 which to goes for?

Thread Summary

The user inquires about selecting between LT1764A and LT1764, noting the LT1764A's stability with ceramic output capacitors. The support engineer recommends the LT1764A for its broader capacitor compatibility and suggests considering the LT3083 as a potentially better alternative.
AI Generated Content

Hi,

LT1764A: stable with ceramic output capacitance with low ESR, while extra consideration must be given to use ceramic output capacitance. 

For LT1764: Recommended ESR is 50mOhm to 3Ohm. You can refer to datasheet for details under "output capacitors and stability" section.

Between LT1764A vs. LT1764, how shall I select and which to goes for? 

  • Hello,

    in general LTC parts with a letter behind the part numbers are improved versions (and younger as well). Here the explanation show the LT1764A is easier to use as it allows ceramic output caps as well (broader choice).

    In general the LT1764/A is quite an old part and there might be better parts in our portfolio:

    LT3083 for example

    kind regards

    Markus

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.