LTM4644-1 LT POWER CAD 3+1 MODEL,

CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.

  • 0
    •  Analog Employees 
    on Apr 27, 2021 12:39 AM

    Hi kdeckstein, 

    Sorry I am unable to attach the example design tool file here. You can also access the LTM4644 3+1 tool (2 outputs) by going to the LTpowerCAD part search page, entering your input voltage range, selecting number of output rails to be 2 and enter the output conditions for the 2 rails (for example 2.5V / 12A for 3-phase rail, 1.8V / 4A for the single phase rail) and then in the 'Find Part #' box you can enter 4644 and click 'Find' and you should see the LTM4644 in the search results to open the design tool for the configuration. 

    Regards,