Post Go back to editing

ADI sim power calc. tool for ADP1972

Dear Sir/Madam,

Do you have the ADI sim power calculation excel file for your new product ADP1972?

I could not find it as following place.

http://www.analog.com/en/content/cu_eval_pmp_tools/fca.html

Thanks Kaos

Parents
  • Here is more information about the ADP1972:

    The ADP1972 was designed for a specific application where both voltage and current control are required. The ADP1972 is a controller without FET drivers or error amplifier. It’s basically a PWM modulator and additional components such as an error amplifier (AD8540 for example) and FET drivers are needed to complete the design.

Reply
  • Here is more information about the ADP1972:

    The ADP1972 was designed for a specific application where both voltage and current control are required. The ADP1972 is a controller without FET drivers or error amplifier. It’s basically a PWM modulator and additional components such as an error amplifier (AD8540 for example) and FET drivers are needed to complete the design.

Children
No Data