Post Go back to editing

ADP1046 capability

Hello,

I consider designing two DC-DC power systems.

One is 2kW power.

     input: 250V~450V

     ouput: 10V ~ 16V, 150A

The second is 10kW.

     input: 350V ~ 450V

     output: 350V ~ 450V, 28A ~ 22A

Is both possible to design with ADP1046?

Best Regards,

Mack

Parents Reply Children
No Data