Post Go back to editing

ADP198 Reverse Polarity Protection

FormerMember
FormerMember

Thread Summary

The user inquired about the ADP198 reverse polarity protection not working as expected when 3.3V is applied at the input and 5V at the output. The final answer explains that the reverse current circuitry requires a Vout to Vin differential of at least 50mV-75mV, which is difficult to achieve if the part is enabled and the 3.3V rail cannot sink current. To ensure proper operation, the EN pin must be driven low before applying 5V to Vout. This applies to similar load switches like the ADP195.
AI Generated Content

Inquiry from customer wanting to better understand the ADP198 reverse polarity protection:

The ADP198 is used with 3.3V at the input and would like to apply a 5V at the output and activate the reverse polarity protection.

It does not seem to work appropriately.

Can you help?

Parents
  • In order for the reverse current circuitry to be activated, the Vout to Vin differential must at least 50mV-75mV.  Normally, if the part is not enabled it is easy for the 50mV differential to be created across an off FET. 

    However, if the part is enabled, this means that the FET is on and the resistance is about 50 milli-ohms.  When the 5V is applied to the output, there is only the 50 milli-ohm resistor between the output and input causing the 3.3V to potentially “float up” to 5V if the 3.3V rail cannot sink current. 

    For the reverse polarity to operate correctly the EN pin needs to be driven low when 5V is present at Vout and before the input is allowed to float high.

    If the EN pin is left high when 5V is applied to the output, over 1A of reverse current will be needed to create this 50-75mV differential and for the ADP198 to engage the reverse polarity protection.

    This also applied to other similar load switched like the ADP195.

    LucaV.


Reply
  • In order for the reverse current circuitry to be activated, the Vout to Vin differential must at least 50mV-75mV.  Normally, if the part is not enabled it is easy for the 50mV differential to be created across an off FET. 

    However, if the part is enabled, this means that the FET is on and the resistance is about 50 milli-ohms.  When the 5V is applied to the output, there is only the 50 milli-ohm resistor between the output and input causing the 3.3V to potentially “float up” to 5V if the 3.3V rail cannot sink current. 

    For the reverse polarity to operate correctly the EN pin needs to be driven low when 5V is present at Vout and before the input is allowed to float high.

    If the EN pin is left high when 5V is applied to the output, over 1A of reverse current will be needed to create this 50-75mV differential and for the ADP198 to engage the reverse polarity protection.

    This also applied to other similar load switched like the ADP195.

    LucaV.


Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.