Post Go back to editing

ADP198 Reverse Polarity Protection

FormerMember
FormerMember

Thread Summary

The user inquired about the ADP198 reverse polarity protection not working as expected when 3.3V is applied at the input and 5V at the output. The final answer explains that the reverse current circuitry requires a Vout to Vin differential of at least 50mV-75mV, which is difficult to achieve if the part is enabled and the 3.3V rail cannot sink current. To ensure proper operation, the EN pin must be driven low before applying 5V to Vout. This applies to similar load switches like the ADP195.
AI Generated Content

Inquiry from customer wanting to better understand the ADP198 reverse polarity protection:

The ADP198 is used with 3.3V at the input and would like to apply a 5V at the output and activate the reverse polarity protection.

It does not seem to work appropriately.

Can you help?