Hello. Can I switch mode LTC3315 when it working?
When my device in wait-mode using burst mode and dynamically set pulse-skip or forced continuous mode. And how much time need to set new mode?
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTC3315A
Recommended for New Designs
The LTC3315A features dual 2A monolithic synchronous step-down converters operating from a 2.25V to 5.5V input supply in one package for space-constrained...
Datasheet
LTC3315A on Analog.com
LTC3315B
Recommended for New Designs
The LTC3315B features dual 2A monolithic synchronous step-down converters operating from a 2.25V to 5.5V input supply in one package for space-constrained...
Datasheet
LTC3315B on Analog.com
Hello. Can I switch mode LTC3315 when it working?
When my device in wait-mode using burst mode and dynamically set pulse-skip or forced continuous mode. And how much time need to set new mode?
The LTC3315 was not specifically designed to switch modes while operating therefore we do not recommend to do this. However we also did not observe any issues switching modes when operating during evaluation at room temperature. Full testing under all conditions has not been done for switching modes when operating.
I do not know the worst case time to accurately switch modes. Once in FC mode from burst mode it can take the regulator 3 to 4 clock cycles to adjust from a high output ripple. This can be evaluated with a demo board on the bench if desired.