ADP1047/1048

Dear Sir,

There are some questions about the ADP1047/1048. Please kindly help advise.

Thanks.

1. There are two OT fault flags in the Flag setting in GUI. What differennce between them?

2. If the RTD pin direct connect to GND, whether it has no OTP function?

3. If the ILIM pin is open, whether it has no fact OCP fuction?

Thanks.

Best regards

NC

Parents
  • Hi NC,

    See the answers bloew.

    1. There are two OT fault flags in the Flag setting in GUI. What differennce between them?

    one is OT_warning and the other is OT_fault. the OT_warning is for warning only and it will take no action. OT_fault is used for OT protection.

    2. If the RTD pin direct connect to GND, whether it has no OTP function?

    yes.

    3. If the ILIM pin is open, whether it has no fact OCP fuction?

    yes. but we do not recommend to so that. if you do not want the fast ocp function, please conect the pin to ground.

    James

Reply
  • Hi NC,

    See the answers bloew.

    1. There are two OT fault flags in the Flag setting in GUI. What differennce between them?

    one is OT_warning and the other is OT_fault. the OT_warning is for warning only and it will take no action. OT_fault is used for OT protection.

    2. If the RTD pin direct connect to GND, whether it has no OTP function?

    yes.

    3. If the ILIM pin is open, whether it has no fact OCP fuction?

    yes. but we do not recommend to so that. if you do not want the fast ocp function, please conect the pin to ground.

    James

Children
No Data