ADP1047/1048

Dear Sir,

There are some questions about the ADP1047/1048. Please kindly help advise.

Thanks.

1. There are two OT fault flags in the Flag setting in GUI. What differennce between them?

2. If the RTD pin direct connect to GND, whether it has no OTP function?

3. If the ILIM pin is open, whether it has no fact OCP fuction?

Thanks.

Best regards

NC

  • Hi NC,

    See the answers bloew.

    1. There are two OT fault flags in the Flag setting in GUI. What differennce between them?

    one is OT_warning and the other is OT_fault. the OT_warning is for warning only and it will take no action. OT_fault is used for OT protection.

    2. If the RTD pin direct connect to GND, whether it has no OTP function?

    yes.

    3. If the ILIM pin is open, whether it has no fact OCP fuction?

    yes. but we do not recommend to so that. if you do not want the fast ocp function, please conect the pin to ground.

    James

  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:43 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin