Hi ,
Can you suggest the best component you have for the following descriptions,
1. DC DC buck regulator(9 V to 5 V)- Input spread voltage range preferred- 6 A Output Current
2. DC DC buck regulator(5 V to 3.3 V)- Input spread voltage range preferred- 3 A Output Current
3. Power ORing Circuit for USB PD ports We are designing our product with two USB PD ports.
One of them is used as Wall charger port and other one is used for PD by Laptops. So, Can you suggest ORing circuit to detect these ports and select output from these rails
---
Thanks & Regards,
Akshay V
format
[edited by: Akshay Vavukkal at 4:59 AM (GMT -4) on 25 Mar 2021]