Post Go back to editing

wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection. The customer wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

  • Hello,

    sometimes page one of the datasheet contains the answer:

    The LT8708-1 always operates as a slave to the master LT8708 and has the capability of delivering as much cur-rent or power as the master.

    Hence I would state, that LT8708-1 can NOT work alone.
    You should check with your customer why they're asking, Especially as LT8708 does exist and would do the job flawless. The LT8708 is the main part for the application, LT8708-1 jus a possible 'add-on'

    kind regards

    Markus