Post Go back to editing

ADP323 Pulsing Spikes

Thread Summary

The user is experiencing 4Hz AC spikes of ±20mV on GND, VIN, and all Vout lines when pulsing EN1 at 4Hz using an MCU. The final answer suggests that the issue is likely due to fast rise and fall times of the EN1 signal, causing common mode noise. Slowing the EN1 pulse edges with an RC filter and reducing the output voltage divider resistances by a factor of 10 may help. Additional input capacitance may also be needed to handle transient currents.
AI Generated Content

I have the schematic below, which i have created with the ADI Linear Regulators Excel tool.

I am producing Vout 1 = 2.8 Volts

                         Vout 2 = 2.5 Volts

                         Vout 3 = 1.8 Volts

I am pulsing the EN1 at 4Hz to drive a circuit but pulsing AC spikes exactly at 4Hz appear at the GND, VIN, Vout 1, Vout 2 , Vout 3  , around -/+20mV .

 

Can you please help me eradicate that issue as soon as possible.

I am not exactly sure what is causing the issue, I am pulsing the EN1 directly from a pin of a MCU.

Thanks in advance.

  • Can Anyone please answer the previous question, if can be done...

    Thanks.

  • There may be a couple issues here.

    I assume the EN1 signal has very fast rise and fall times.  This could be injecting noise into the ground and causing the noise to appear.  It may be common mode signal since you are seeing on GND.

    Can you put a scope probe on GND and short the probe ground connection to the scope input when measuring the noise on the GND?  If you still see the spikes, it is definitely common mode noise, not differential mode noise.  This isn't really an issue unless your circuit has poor common mode rejection.  Slowing the EN1 pulse edges with an RC should help.  Try to limit the rise and fall times to a few microseconds or longer.

    I noticed that the output voltage divider resistances are very high.  Is it possible to reduce them by a factor of 10?  This also might help reduce the coupling of the EN1 signal into the output.

  • Do you have a load on the output of Vout1. If you load is demanding a lot of current then you may be forcing a transient at the input of the LDO. You may need additional input capacitance.

    Also since the output cap is being charged when you disable it, the input cap is sourcing current to recharge it when you re-enable the LDO, again higher input cap may be needed in this case.

    LucaV

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.