My question is regarding the DC1962C demo board. I'm using LT power play to communicate with it via the DC1613A programming pod.
I looked at the schematic and saw for the LTC2974, the ASEL1 pin is tied LOW and ASEL0 is tied HIGH. The Address look-up table (Table 1) on the LTC2974 datasheet says this would correlate to a 7-bit hex base address of 0x5E. But LTpowerplay tells me that the LTC2974 on the demo board detects a 7-bit hex base address of 0x32. I was wondering if there was something I’m overlooking? Trying to understand why the software wouldn’t show 0x5E. An Post y help is appreciated!