ADP2164 and ADP2164-1.8

Hi,

I am using one of regulator ADP2164 in my circuit to generate 1.8 V from 3.3 V input. unfortunately i mounted ADP2164ACPZ-1.8 instead of ADP2164APZ. As per my circuit i used feedback resistors to adjust and i mounted the which has fixed output voltage. Will it work or not? or will affect to another stages. I attached circuit of my board.

same case about ADP1755 also, this one is used to generate 1.3 V from 1.8 V input.

Regards,

Ravi