Post Go back to editing

LT3471 Negative Supply

I have designed a ±20V power supply using this device and I have used the same design on a previous board which worked well. This time I am using an increased power supply (from 8V to 12V) and the only other change is the input capacitor was swapped for an electrolytic of the same value. When I tested the power supply the positive side works but the negative side was drawing a lot of current and the output was 0V. I tried a couple different capacitor values at C58 and after a couple tests put the value back to the original value to get images from probing of the switching node however at that stage it completely burnt itself out and I am now measuring 8Ω between SW2 and GND. I can't understand why this circuit worked in the previous design and not in this one. Any advice or indication what is causing this problem would be greatly appreciated.

Parents Reply Children
No Data