Post Go back to editing

Looking AC/DC converter evaluation board

Hi!

 

Currently I am searching for several Offline AC/DC Evaluation Board (SMPS) to buy with following requirements:

  1. Universal input (85 – 264 Vac)
  2. +PFC block is OK
  3. Output:
    1. 48V  with power over 400W
    2. 5V with power below 300W

are there any available evaluation board or references that meets my requirements? Where can i see lists of your offline eval board?

Thanks in Advance

Catur

  • Hello, Catur.

    For PFC with universal input, you may want to look at ADP1047 and ADP1048. PFC evaluation boards (300W and 600W) are available.

    Other PFC controllers can be found here.

    About the DC-DC block, you may refer to ADP1046A. Evaluation boards are also available.

    You may also want to view the following related parts for DC-DC block:

    ADP1052, ADP1055, ADP1050, ADP1051, ADP1053, LT3798

    Documentations such as datasheets, user guides and reference materials can be found on the corresponding product pages.

    Those should be helpful for designing offline, isolated SMPS.

    Thanks and BR,

    Migs