Hi
Would you tell me the min/max value of Short-Circuit Current of LTC3245.
If it is not possible to disclose the design value, could you tell me reference data?
Best Regards,
LTC3245
Recommended for New Designs
The LTC3245 is a switched capacitor buck-boost DC/DC converter that produces a regulated output (3.3V, 5V or adjustable) from a 2.7V to 38V input. The...
Datasheet
LTC3245 on Analog.com
Hi
Would you tell me the min/max value of Short-Circuit Current of LTC3245.
If it is not possible to disclose the design value, could you tell me reference data?
Best Regards,
Hi support team
Would you tell me the status of this question?
Best Regards,
Hello, I do not have min and max values at the moment but looking at data for over 204k pcs over temp to parts for this test the short circuit current ranges from 690mA to 960mA for ±6 sigma. This is with VIN @ 12V and VOUT @ 0V.
Hi MartyM-san
Thank you for your reply.
This information is helpful for our support.
Best Regards,