Hi,
I use LT3956 led driver for back light driver. LED driver will be work 9-36V supply voltage. My LED parameters are 14,3V @ 600mA. I try to simulate circuit but I can not find needed parameters.
Could you please help me for this.
Hi,
I use LT3956 led driver for back light driver. LED driver will be work 9-36V supply voltage. My LED parameters are 14,3V @ 600mA. I try to simulate circuit but I can not find needed parameters.
Could you please help me for this.
Hi
Can you elaborate of the parameters you cannot find ?
Regards
Hi Mikee,
I draw a simulation circuit on LTSPICE.
My common problem is, my circuit can not work on buck mode. Our design have to work 9 to 36V supply voltage,
When i apply 12V input voltage, circuit work fine. (Bost model OK)
When i apply 36V input voltage, i can not control output current. (Buck mode)
I am getting 7A output current.
My display parameters are Vf=14,3V IF=600mA
Could you please help on simulation circuit. Because I produced this circuit and does not work correctly.
I have another question. LT3956 works with the same hardware configuration Buck and Boost mode? Or it works with different hardware schemes.
Hi
The circuit you are currently using is for the boost configuration.
For the buck-boost operation please refer to sample circuit on page 17
and SEPIC sample on page 18 of the data sheet
Regards
On page 18 SEPIC sample with simuation work fine.
On page 18 SEPIC sample with simuation work fine.
Thank you for support.
Yes. i solved my problem. Thank you for support.