Post Go back to editing

ADI LED driver product for individual string control ?

Hi,

Just a simple question that can ADD5211 or ADP8140 control dimming individually on each of multi strings of LEDs ?

If not, please let me know any products can have individual string control ?

Best Regards,

Parents
  • Hello Takehisa,

    No, the ADD5211 or ADP8140 cannot control each string individually.  However, the ADP8140 can be easily connected in parallel, so that you can control up to 2A of LED current individually on each ADP8140.  But it requires a separate IC for each LED string. 

    To control multiple individual strings with one IC, you can use the ADP8860/1/3, ADP8870, or ADP8866.

    Best Regards,

    - Jon

Reply
  • Hello Takehisa,

    No, the ADD5211 or ADP8140 cannot control each string individually.  However, the ADP8140 can be easily connected in parallel, so that you can control up to 2A of LED current individually on each ADP8140.  But it requires a separate IC for each LED string. 

    To control multiple individual strings with one IC, you can use the ADP8860/1/3, ADP8870, or ADP8866.

    Best Regards,

    - Jon

Children
No Data