Hi all,
This is an inquiry about how to use the LT3466.
I would like to use only one of the two channels.
How should I handle the SW2, Vout2, FB2, and CTRL2 pins that are not used?
Best Regards,
Thanking you.
LT3466
Production
LT3466 is a dual full function step-up DC/DC converter specifically designed to drive up to 20 White LEDs (10 in series per converter) with a constant...
Datasheet
LT3466 on Analog.com
Hi all,
This is an inquiry about how to use the LT3466.
I would like to use only one of the two channels.
How should I handle the SW2, Vout2, FB2, and CTRL2 pins that are not used?
Best Regards,
Thanking you.
Hi Takahiro,
You may leave those converter #2 pins (SW2, VOUT2, FB2 and CTRL2) open.
However, I recommend to use LT3465 instead of LT3466 if you are driving 6 or less LEDs.
Regards,
Xian
Hi Takahiro,
To be on the safe side, best to ground CTRL2 to make sure the converter is off. Other pins can be open.