Post Go back to editing

LT8392 Design

Hi!

I came across the LT8392 when looking for some different buck boost regulators. I am wanting to know if the LT8392 is capable of providing the necessary requirements for my design. 

Vin: 4.5 - 60 V

Vout: 4.5 - 42V

Imax: 8A

I am more interested in making sure this would be able to handle the higher power applications, such as 42V output at 8A, or around 330W in general. It would also be great if I could get some potential design values to go along with this, if the LT8392 is capable of meeting my power requirements. Most of the data sheet has it listed no higher than 125W. 

Thanks!