Post Go back to editing

Comparison of two dual +-V output converter circuist: LT1930 vs LT8335

Hi,

I am studying on dual ouput converter based on SEPIC topology. I find from datasheets that both LT1930 and LT8335 could create a symmetrical dual output. Please see.

The pictures show clear that there are 2 kinds of circuts to create dual +-V outputs.

1, consists of 1 inductor and 4 Schottky diodes.

2, consists of 3 inductors (coupled) and 2 Schottky diodes.

My questions are:

Is the 2 circuits equivalent?

If they are quite different, what's the exact differences about their efficiency and output current capacity?

Is there a simple sign via which I could easily judged which kind of ICs should use which circuit?

Thank you very much!

Best Regards.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.