Can the LT3797 be configured sot hat one of it's outputs is used as a simple buck regulator? Only 2 LED drivers needed, and wondering if the 3rd could be configured to step down the 24V input to a 5V output to power an RS422 interface?
Thank you!
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
LT3797
Production
The LT3797 is a triple output DC/DC controller designed to drive three strings of LEDs. The fixed frequency, current mode architecture results in stable...
Datasheet
LT3797 on Analog.com
Can the LT3797 be configured sot hat one of it's outputs is used as a simple buck regulator? Only 2 LED drivers needed, and wondering if the 3rd could be configured to step down the 24V input to a 5V output to power an RS422 interface?
Thank you!
Hi Ted
Yes, you can configure it as described
Regards
Thankes Mikee, are you familiar with any example circuits that would show how to do this?
Thankes Mikee, are you familiar with any example circuits that would show how to do this?
Hi Ted
You can use figures 11 to 13 of the data sheet as reference.
If your buck needs to have the same GND as the controller I would recommend using it in SEPIC mode instead
Regards