Post Go back to editing

LT1930 Dual Output Converter Topology

Hi,

I notice that LT1930 has a special output circuit (datasheet P8).

How can I calculate the valus as Vin, L1, Iout, Vout, C1 and C2 if I want to change them?

For instance, I need 12V input while dual 18V ouputs.

It seems that the method and fomula are not mentioned in the part of operations.

Is it essentially a SEPIC topology?

What do the diodes D2 and D4 play in that place? Are they equivalent to inductors?

Finally, can this topology be applied to LT1935 and LT3489?

Thanks.

Best Regards