ADP3339
Not Recommended for New Designs
NEWER ALTERNATIVES:
ADM7172: 6.5 V, 2 A, Ultralow Noise, High PSRR, Fast Transient Response CMOS LDO
The ADP3339 is a member of the ADP33xx family of precision...
Datasheet
ADP3339 on Analog.com
According to the datasheet ADP3339 has a 2.8 V to 6 V input voltage range. We currently use this device in our design which feed in only 2.48V at the input due to design limitation. I understand that this is not ideal but so far we have minimal fall-out. Without specifying in a new part, could someone please explain the impact of providing insufficient input power and the risk/failure symptoms?
Thanks.
Peter