Post Go back to editing

ADP1761 does it support 3.3V logic enable and power good?

Hello,

I'm implementing an ADP1761 and the power sequencer circuit has 3.3V logic IO levels. Reading the datasheet, it looks like ADP1761 would tolerate a direct 3.3V level to its enable input (the absolute maximum rating for the pin is 3.96V). That's also the case for the PG pin, that would be pulled up to 3.3V and it seems to withstand up to 3.96V absolute maximum.

However, I can't find nominal ratings for these pins and 3.3V is close to the absolute maximum of 3.96V. Can I use 3.3V IO levels to safely enable and pull-up the power good pin of an ADP1761?