Post Go back to editing

ADM1075 DEVICE ADDRESSING

Hello

If would like to use ADM1075 usage 5 in a system that means I should use ADM1075-1 , ADM1075-2 in the same time here?

As I checked the datasheet that information below

DEVICE ADDRESSING

The ADM1075 is available in two models: the ADM1075-1 and ADM1075-2. The PMBus address is seven bits in size. The upper five bits (MSBs) of the address word are fixed and are different for each model, as follows:

• ADM1075-1: Base address is 00100xx (0x10)

• ADM1075-2: Base address is 00110xx (0x18)

Or I missing anything for this request? any comments, thanks

Parents Reply Children
No Data