Dear Sir/Madam,
Our customer is studying to use Ir-LED driver with your white LED driver like a ADP8140.
So what is the notes to use as Ir-LED driver?
Only Vf difference?
Why are your LED drivers designed for white LED only?
Thanks Kaos
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADP8140
Production
The ADP8140 provides high current control of up to four LED drivers. Each driver can sink up to 500 mA. The sink current is programmed for all four drivers...
Datasheet
ADP8140 on Analog.com
Dear Sir/Madam,
Our customer is studying to use Ir-LED driver with your white LED driver like a ADP8140.
So what is the notes to use as Ir-LED driver?
Only Vf difference?
Why are your LED drivers designed for white LED only?
Thanks Kaos
HI John,
Thanks your your kindly answer for this.
I am clear about your LED drivers.
OK, I will visit our customer and recommend your good LED drivers which are able to use for any Ir- LEDs.
In fact, customer needs the following rating.
type #1, 4 LEDs , per 60mA
type #2, 1 LED, 600mA
He is testing type #1 and type #2.
That Ir-LED will be used for lighting IR-camera security.
So the current will flow continuously max 24hours/day .
I can update the result after visit customer later.
Thanks Kaos
Hi Kaos,
Actually, nearly all of ADI's LED drivers can be used to drive any LED. You can see the list here:
https://www.analog.com/en/products/power-management/display-and-lighting.html
The only exception is the ADM8843 and ADM8845, which are intended to drive LEDs with a forward voltage (Vf) between 3 and 4.5V. Other than that, any of these ICs will work well with IR LEDs. Often times, our IR LED customers are looking for higher current drives, and if that is the case for you, then I would recommend to start with looking at the ADP8140 and the ADD5211. The ADP8140 is a 4 channel, high current, feature rich and incredibly flexible LED controller. It can be used in nearly any topology or application. The ADD5211 is a multi channel, 800mA (total LED current), high voltage, boost regulator. Please let me know if you have any questions about these parts. Or if you would like to do something that you don't see a good solution for.
Best Regards,
Jon Kraft