Post Go back to editing

Can I use the ADP1872 to design a bidirectional converter?

The ADP1872 is synchronous buck controller. Theoretically, synchronous buck converters can be used as bidirectional converters.  So keeping that in mind the ADP1872 should also be bidirectional (i.e it should be able to deliver current from and to both sides if required). Is it so ?




Thank you!

Parents
  • Thanks Kevin,

    I couldn't find anything in the ADP1872 datasheet explaining if it can be used as a bidirectional converter or not. Can it really work in the bidirectional mode (buck mode when current is flowing from the input to the output, and boost mode when current is flowing from the output to the input) ?

    Thank you ,

    Dhiogo

Reply
  • Thanks Kevin,

    I couldn't find anything in the ADP1872 datasheet explaining if it can be used as a bidirectional converter or not. Can it really work in the bidirectional mode (buck mode when current is flowing from the input to the output, and boost mode when current is flowing from the output to the input) ?

    Thank you ,

    Dhiogo

Children
No Data