Post Go back to editing

ADP1853 power-up simPE model

Hello.

Do you have power up simPE model of ADP1853?

ADP1853 simPower don't have export menu of start-up
And I tried to make start-up model using the export SimPower model, but didn't go well.

I want to know soft-start and Pre-charge simulation.

best regard.

Parents
  • Hello.

    Thank you for your sim data.

    Immediately, I tried the simulation.

    My customer's request current is 2A~10A, it changed the load.

    The result is an attached graph.

    However, because at light load there was ringing. I tried to optimization.

    My customer request is Vin=12V~3.3V Vout=1.2V,Iout=2A~10A.

    I tried to optimize in this condition.

    Finally, I introduced the circuit conditions from ADIsimPow.

    Ringing was suppressed by the phase compensation of the entire circuit.

    Soft-start was a result of similar calculation values.


    But I have a question, that Why flat Voltage output appears, is it dependent on the input voltage ?

    Best Regards,

Reply
  • Hello.

    Thank you for your sim data.

    Immediately, I tried the simulation.

    My customer's request current is 2A~10A, it changed the load.

    The result is an attached graph.

    However, because at light load there was ringing. I tried to optimization.

    My customer request is Vin=12V~3.3V Vout=1.2V,Iout=2A~10A.

    I tried to optimize in this condition.

    Finally, I introduced the circuit conditions from ADIsimPow.

    Ringing was suppressed by the phase compensation of the entire circuit.

    Soft-start was a result of similar calculation values.


    But I have a question, that Why flat Voltage output appears, is it dependent on the input voltage ?

    Best Regards,

Children
No Data