Customers want to use LTC4151HDD#PBF or LTC4151HMS#PBF (Max 125 degrees).
However, it is labeled LTC4151-1 in Figure 9.
Please check if the same can be used for LTC4151HDD#PBF or LTC4151HMS#PBF.
Figure 9.Opto-Isolation of the I2C Interface Between LTC4151-1 and a Microcontroller (1.5kHz Data Rate of I2C is Limited by Slew Rate of Opto-Isolators)