Post Go back to editing

Question of LTC4151 (I2C Isolation)

Customers want to use LTC4151HDD#PBF or LTC4151HMS#PBF (Max 125 degrees).

However, it is labeled LTC4151-1 in Figure 9.
Please check if the same can be used for LTC4151HDD#PBF or LTC4151HMS#PBF.

Figure 9.Opto-Isolation of the I2C Interface Between LTC4151-1 and a Microcontroller (1.5kHz Data Rate of I2C is Limited by Slew Rate of Opto-Isolators)

Parents Reply Children