Post Go back to editing

What is the output current of ADP3335 MSOP ?

Dear sir.

What is the maximum output current of ADP3335ARMZ-3.3-RL(MSOP) ?

Even theoretical maximum current of ADP3335 MSOP is 300mA.

As I checked, it just can be maximum 100mA.

Its condition is below.

Input voltage is 5V

Output voltage is 3.3V

Ambient temperature is 35 Cels. degree.

Parents Reply Children
No Data