Post Go back to editing

What is the output current of ADP3335 MSOP ?

Dear sir.

What is the maximum output current of ADP3335ARMZ-3.3-RL(MSOP) ?

Even theoretical maximum current of ADP3335 MSOP is 300mA.

As I checked, it just can be maximum 100mA.

Its condition is below.

Input voltage is 5V

Output voltage is 3.3V

Ambient temperature is 35 Cels. degree.

Parents
  • Hi Kiyoung SON,

    The max load current is typically 800mA, and the specifications table in the ADP3335 datasheet show regulation and noise values for up to 500mA of output current.

    You might be seeing a different issue, can you share some scopeshots of the failure and your schematic?

    Best regards,

    Jess

Reply
  • Hi Kiyoung SON,

    The max load current is typically 800mA, and the specifications table in the ADP3335 datasheet show regulation and noise values for up to 500mA of output current.

    You might be seeing a different issue, can you share some scopeshots of the failure and your schematic?

    Best regards,

    Jess

Children
No Data