Post Go back to editing

ADP1614; Largest SS capacitor allowed?

What is the largest capacitor that can be used on the Soft Start pin of the ADP1614? It contains an internal low-side switch to reset the capacitor in response to certain events (such as thermal shutdown) which implies that there is an upper board on the size of the soft-start capacitor, but the datasheet is silent. I'm looking to use a very long soft start time (~250ms), which, in turn, requires a 1uF cap or so.